AnsweredAssumed Answered

bug report for X-CUBE-SPN7

Question asked by blue.andy on Jun 13, 2018

Hi ST support and developer,

  I have a small bug report for X-CUBE-SPN7, in the project of examples, 

  Projects/Multi/Examples/MotorControl/SW4STM32/STM32F302R8-Nucleo,  the include path has set to

../../../../../../Drivers/BSP/Components/L6230  , instead of ../../../../../../Drivers/BSP/Components/l6230 :

  This causes build failed on Linux.

  On Windows it is OK as Windows could treat 'L' and 'l' to be same in the path and file name, but Linux will see them different.

 

-Andy

Outcomes