AnsweredAssumed Answered

SWV on the STM32F746ZG

Question asked by Luka Mesaric on Jun 12, 2018
Latest reply on Jun 13, 2018 by Luka Mesaric

Hi, I am trying to enable the SWV on the STM32F746ZG, but without success. I generated the code with CUBEMX (enabled the Trace asynchronous SW) and in debugger configuration configured interface SWD, and trace SWV (with core clock at 200MHz). I have also configured the trace configuraton in debugger, but when i click start trace, no data is shown. In the console window I get verify failed message. I am using J-Link.

Outcomes