AnsweredAssumed Answered

LIS2DW12 INT1?

Question asked by vitthal muddapur on Jun 9, 2018

Hi,

 

i am working on stm32l071, interfacing with LIS1DW12 i have configured 

1. Write 64h in CTRL1 // Turn on the accelerometer // ODR = 200 Hz, High-Performance

2. Write 04h in CTRL6 // FS 2 g LOW_NOISE enabled

3. Write 20h in CTRL7 // Do not use low-pass filter for 6D, enable interrupts

4. Write 40h in TAP_THS_X // Set 6D threshold (6D_THS[1:0] = 10b = 60 degrees)

5. Write 80h in CTRL4_INT1_PAD_CTRL // 6D interrupt driven to INT1 pin

6. write 10h in CTRL3 

 

getting satus SIXED register change the direction of 6D

 

but didn't get interrupt in MCU from INT1 LIS2DW12 

Outcomes