AnsweredAssumed Answered

Run VL53L0X at lower voltage than specified?

Question asked by guillem cabo on Jun 11, 2018

Hi, the specifications of the  VL53L0X said that recommended input voltage is between 2.5 and  3.5V
I have test it on a prototype at 2V and works fine at short range  (150 mm). 

Which problems can i experience?
If the only problems is  have a reduced range or less accurate measurements it's fine. It will be only on for a few samples  and it will be turned of through Xshut pin.


Outcomes