AnsweredAssumed Answered

STM32F429 Stuck in GUI_init() after generation using STM32cubeMX V4.26

Question asked by barkana abdel on Jun 11, 2018
Latest reply on Jun 14, 2018 by Vitaliy Chernobay

Hi guys, I'm using STM32CubeMx V4.26 to configure STM32F429 that is connected to TFT LCD. I m trying to get my TFTLCD to work with StemWin using FreeRTOS. My program compile and link smoothly without problem. Running the program in the hardware leads to an MCU stuck in the function : GUI_init()

I ve checked some similar issues and it looks to be related to the graphic library and RCC clock.

 

Could any one have guidance for this issue ? are there some sample code ? 

Outcomes