AnsweredAssumed Answered

QSPI: Write/Read strings from QSPI memory

Question asked by Rick MC on Jun 6, 2018
Latest reply on Jun 8, 2018 by Clive Two.Zero

Hello,

I implemented some functions to read and write the QSPI memory by using functions HAL_QSPI_Transmit() and HAL_QSPI_Receive() provided by the libraries.

 

Everything works fine. I just wonder how I can write and read strings using these functions.

I want to write:

   char myString[100][50];

but the above functions have a uint8_t as an input!

 

Is there any way to do so, other than passing a single character at a time?

Thanks,

Outcomes