AnsweredAssumed Answered

Need I/O controller EVM board

Question asked by Md Mubdiul Hasan on Jun 5, 2018
Latest reply on Jun 22, 2018 by AvaTar

Hi there,

 

I have been back to high power design.

My system contains 3phase, 380V, 50Hz  ac input, secondary surge protector, Aux Tr ( single phase, 380V/220V, 300VA), phase transformer( 3ph, 380v/12v,0v,12v,100VA) and a main transformer ( 3ph, 380V/9V,18V,800VA),

SCR(1600V, 50A) bridge, DC reactor( DC 20V,20A). Rectifier output should be DC 20V 20A.

 

My requested EVM should be,

 

1. PTR secondary windings  phase, amplitude and rating controller.

2. MTRs secondary fuse (690V, 32 A)  sensing 

3. SCRs switching controller.

4. 50mlV, 30A shunt sensing,

5. GPS communication,

6. RSM 

7. LAN

8. Display....etc,

 

 

Kindly recommend me one.

You can also transfer this post to suitable forum.

 

Regards

Hasan

Outcomes