AnsweredAssumed Answered

STM32 ADC DMA without Interrupt

Question asked by benjamin Gräf on Jun 1, 2018
Latest reply on Jun 6, 2018 by benjamin Gräf

Hello!

 

Is it possible to use the ADC in DMA mode without enabling the interrupt? I really do not need the interrupt because it will block the rest of my programm, which is very important to not be blocked. The ADC runs very fast and therfore many interrupts occur. The DMA writes the value of the ADC into a variable in the RAM storage. So why use an interrupt, I just read the value in my main programm. 

 

I am using CubeMX for configuration.

 

best regards,

 

Benjamin.

Outcomes