AnsweredAssumed Answered

Is it possible to work I2C fast mode(400KHz) and USB FS together in STM32F103VCT6

Question asked by sruthi on May 31, 2018
Latest reply on Jun 6, 2018 by sruthi

I want to use I2C fast mode(400KHz) and USB full speed mode in parallel. My controller is STM32F103VCT6. In reference manual I had read that for USB we must use 48MHz clock and also for I2C fast mode communication  i2c clock frequency must be a multiple of 10MHz . I'm not able to set a sysclk compactable for these two peripherals. Is there any solution for this? Please help...

Outcomes