AnsweredAssumed Answered

System Workbench for STM32 : problem to import project from cubemx

Question asked by christophe trichet on May 31, 2018

Hello,

generally i have problems importing project example from cubex repository.

1° i lauch the System Workbench for STM32 with a workspace on c:\workspace

2° i import the cubex project by File->import->genral-> existing project into workspace -> browse -> C:\Users\..\STM32Cube\Repository\STM32Cube_FW_F4_V1.18.0\Projects\STM32F429I-Discovery\Applications\STemWin

2 projects are proposed so i select both (hello world + sample demo)

 

Then i have the warning some project cannot be imported because they already exist.

 

How can i do to import the 2 projects into System Workbench for STM32 ?

 

thanks

best regards

System Workbench for STM32 - Copie

Outcomes