AnsweredAssumed Answered

STM32 PMSM FOC on STM32F107

Question asked by suslov.andrej on Sep 22, 2014
Latest reply on Sep 29, 2014 by Gigi
Hello guys,

I am trying to use STM32 PMSM FOC v3,4 with STM32F107VCT6 MCU. Is it possible?

I previously used the library with STM32F103 mcu. I compared the f107 with f103 and found that they are almost the same (except 107 has more peripherals). So I used the same configuration as was on f103, but the board is not responding. 

I noticed that f107 has 25MHz oscillator, but in ST motor control workbench there is only 8MHz option.

 Could this be the problem? Is there any way to fix this? Or simply f107 can't be used with PMSM FOC library?

Thank you for your responses and help.

Have a nice day.

Outcomes