AnsweredAssumed Answered

ST link V2

Question asked by izal muin on May 29, 2018
Latest reply on May 29, 2018 by Imen D

I need to program external memory using CLI. Conventional programming using the software is succesfull. Need to integrate the commands for the labview programming.

 

 

C:\Project\Programming\ST-LINK Utility>ST-LINK_CLI.exe -P assets.hex -EL MX25L512G_STM32F769I-DISCO.stldr
STM32 ST-LINK CLI v3.0.0.0
STM32 ST-LINK Command Line Interface
ST-LINK SN : 48FF6C067266535216230367
ST-LINK Firmware version : V2J29S7
Connected via SWD.
SWD Frequency = 4000K.
Target voltage = 3.1 V.
Connection mode : Normal.
Device ID:0x451
Device flash Size : 2048 Kbytes
Device family :STM32F76x
Loading file...
Flash Programming:
  File : assets.hex
  Address : 0x90000000
  External Loader File : MX25L512G_STM32F769I-DISCO.stldr
  Device Name          : MX25L512G_STM32F769I-DISCO
  Device Start Address : 0x90000000
  Device Size          : 0x04000000
  Device Type          : Nor Flash
Memory programming...
¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦ 0%
Timeout during flash programming
Error occured during erase operation!
Programming Complete.
is the  any additional parameter need to be type into it?  I have tried with the latest version seem not succesfullly done both using the GUI or CLI 

Outcomes