AnsweredAssumed Answered

see where my prgm finish in the flash memory

Question asked by TARHAN SAMAH on May 24, 2018
Latest reply on May 24, 2018 by Clive Two.Zero

hello evry one when i program my stm using keil ,, i want to see where is the adress that my sofware ended at 

in the flash memory 

 

 

just got this 

 

*** Using Compiler 'V5.06 update 4 (build 422)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'
Build target 'ETHERNET-STM32F429ZI'
compiling eth.c...
linking...
Program Size: Code=55696 RO-data=1132 RW-data=664 ZI-data=76736
"ETHERNET-STM32F429ZI\ETHERNET-STM32F429ZI.axf" - 0 Error(s), 0 Warning(s).
Build Time Elapsed: 00:00:14
Load "ETHERNET-STM32F429ZI\\ETHERNET-STM32F429ZI.axf"
Erase Done.
Programming Done.
Verify OK.
Application running ...
Flash Load finished at 15:23:06

and i see in blue increasing a browser but very fastly so  i cannot get the end adress ??

 

 

is there a way to see the end adress ????

 

thanks 

Outcomes