AnsweredAssumed Answered

Issue with ADRDY of  ADC1_ISR register on NUCLEO-H743ZI ADC1

Question asked by Deepak Soni on May 24, 2018

Hi, I am trying to use NUCLEO-H743ZI ADC1, I am following the procedure that is recommended in the reference manual, getting out of deep power down, turning on and waiting for voltage regulator to stablize and then confirming these two things are happening. After this when I set ADEN bit of ADC1->CR register and polling for the ADRDY of  ADC1_ISR register, it is not getting set, means adc is not getting ready. I haven't changed any clock or power setting those are running in post reset default state. I am attaching my whole program with the library I am using, pease help me with this.

Thank You

Attachments

Outcomes