AnsweredAssumed Answered

Cannot compile STM32Cube's BSP example - missing header

Question asked by Jur Div on May 24, 2018
Latest reply on May 24, 2018 by Jur Div

Hello!

 

I am trying to compile the BSP example provided in STM32Cube_FW_F7_V1.11.0/Projects/STM32746G-Discovery/Examples/BSP , but I get the following error: src/log.c:38:10: fatal error: lcd_log.h: No such file or directory

 

There is a comment block (in the lcd_log_conf.h) which says:

******************************************************************************
* @file BSP/Inc/lcd_log_conf.h
* @author MCD Application Team
* @brief lcd_log configuration template file.
* This file should be copied to the application folder and modified
* as follows:
* - Rename it to 'lcd_log_conf.h'.
* - Update the name of the LCD driver's header file, depending on
* the EVAL board you are using, see line40 below (be default this
* file will generate compile error unless you do this modification).
******************************************************************************

 

I don't know what name should I update, since there is nothing really on line 40 and the file included:

#include "stm32746g_discovery_lcd.h"

 

Where can I find the missing header file lcd_log.h?

Outcomes