AnsweredAssumed Answered

bSwitching ON/OFF two devices using two BTA06 but same Line

Question asked by Engg Try on May 24, 2018

Dear All,

 

I have been working on a project where I need to Switch on Two devices using Two BTA06 controlled by Digitally Opto-Triac. Line and Neutral are same for both.

 

Attached is the schematic.

 

I have issue that when I swithch ON Triac 1 and keep Triac 2 OFF still I get 120V output on triac2 which should be zero.

However, switching OFF Triac 1 voltage is gone.


Can you please suggest what could I have missed?

Attachments

Outcomes