AnsweredAssumed Answered

STM32H743BIT ETHERNET UDP PACKET RECEIVING

Question asked by maheshwar reddy on May 23, 2018

Hai ,

        We  are using the STM32H743BIT controller . we are using  the cubemx to generate the code for the  ethernet . In our application we need to receive the UDP packet  which function we need to use . To send the UDP packet we are using the (UDP_packet_send(uint8_t *Tx_buf,uint16_t length))  function . Before this we are using the STM32F743BIT controller . But we took the the data from the (low_level_input(struct netif *netif)) from this function . Now we are not receiving any data .

Thank you.

best regards 

Maheshwar. 

Outcomes