AnsweredAssumed Answered

Use of X-NUCLEO-LPM01A with STM32L072

Question asked by Sujan Nag on May 22, 2018

Hello everyone, 

This is my first post here.

As part of my research with LoRaWAN, I am working on a custom built board having an STM32L072 module. One of the critical sections of my research involves calculating the energy consumption during transmission and reception. Hence I am looking for a method to power the board using 3.3v and log the voltage and current consumption.

 

As so I came across X-NUCLEO-LPM01A. According to its datasheet:

"It can be used to supply and measure the consumption of STM32 Nucleo-32, Nucleo-64 or Nucleo-144 boards, using Arduino connectors. Alternatively, it supplies and measures the consumption of any target connected by wires via the basic connector."

My custom built board simply needs a VCC and a GND to operate. So I was wondering if X-NUCLEO-LPM01A will suffice for this project. I was not able to find any video demonstrating the same. 

 

Please advice.

 

Thanks

Sujan.

Outcomes