AnsweredAssumed Answered

VL53L0X interrupt setting

Question asked by Chandra Mangipudi on May 21, 2018
Latest reply on Jun 15, 2018 by just4you

Hi 

 I am trying to get the VL53L0X using the api provided and the source code available on vl53l0x_api - test | Mbed  which is just a copy of the VL53L0X api. I am using the STM32L432KC NUCLEO board with I2C connnection to a breakout board available on ebay -> VL53L0X Time-of-Flight Distance Sensor Breakout GY-VL53L0XV2 Module for Arduino | eBay  

 The module works fine but the interrupt pin does not do anything. I am trying to use the 0x04 setting for NEW_DATA_READY setting as per the API, but don't see any trigger on the interrupt or on a digital logic analyzer. 

 Please help

 

Best

Chandra

Outcomes