AnsweredAssumed Answered

How to set B-LCDAD-HDMI1's 1024x768 in stm32f769-eval?

Question asked by hungchul.shin on May 19, 2018
Latest reply on May 22, 2018 by hungchul.shin

I am using the stm32f769 - eval board.

  And, I am using the DSI to HDMI adapter.

I am trying to use the ADV7533 to 1024x768 , 16bit on B-LCDAD-HDMI1.

However, I do not know how to set adv7533.

I did a search but there is no related information or documentation.
Do you know how to set parameters?

or,
Can you tell me the parameter value?

I do not know what the MCU used in the following, but it is the data I searched on the internet.

/_________________________________________________________________________________

/*adv7533*/
46  { 640, 480, 96, 2, 48, 16, 33, 10, 25170000, 60},/*640x480p  -1*/
47  { 720, 480, 62, 6, 60, 19, 30, 9, 27000000, 60},/*720x480p  -2*/
48  { 720, 480, 62, 6, 60, 19, 30, 9, 27000000, 60},/*720x480p -3*/
49  {1280, 720, 40, 5, 220, 110, 20, 5, 74170000, 60},/*1280x720p -4*/
50  {1980, 1080, 44, 5, 148, 88, 15, 2, 74170000, 60},/*1980x1080i -5*/
51  { 720, 480, 62, 3, 114, 17, 15, 5, 27000000, 60},/*720x480p -6*/
52  { 720, 480, 62, 3, 114, 17, 15, 5, 27000000, 60},/*720x480p -7*/
53  {1440, 240, 124, 3, 114, 38, 15, 4, 27000000, 60},/*1440x240p -8*/
54  {1440, 240, 124, 3, 114, 38, 15, 4, 27000000, 60},/*1440x240p -9*/
55  {2880, 480, 248, 3, 228, 76, 15, 4, 54000000, 60},/*2880x480i -10*/
56  {2880, 480, 248, 3, 228, 76, 15, 4, 54000000, 60},/*2880x480i -11*/
57  {2880, 240, 248, 3, 228, 76, 15, 4, 54000000, 60},/*2880x240p -12*/
58  {2880, 240, 248, 3, 228, 76, 15, 4, 54000000, 60},/*2880x240p -13*/
59  {1440, 480, 124, 6, 120, 32, 30, 9, 54000000, 60},/*1440x480p -14*/
60  {1440, 480, 124, 6, 120, 32, 30, 9, 54000000, 60},/*1440x480p -15*/
61  {1920, 1080, 44, 5, 148, 88, 36, 4, 148350000, 60},/*1920x1080p -16*/
62  { 720, 576, 64, 5, 68, 12, 39, 5, 27000000, 50},/*720x576p -17*/
63  { 720, 576, 64, 5, 68, 12, 39, 5, 27000000, 50},/*720x576p -18*/
64  {1280, 720, 40, 5, 220, 440, 20, 5, 74170000, 50},/*1280x720p -19*/

________________________________________________________________________________/

 

However, from the performance of DSI, I know that 1024x768 is the best.
I want to set 1024x768, 16bit, RGB565, 2lane .....
Thank you for knowing how to set parameters.

It's difficult ... Hue..ㅠㅠ
 

Outcomes