AnsweredAssumed Answered

STM32F032 CAN bus

Question asked by Yogesh Khedkar on May 18, 2018
Latest reply on May 25, 2018 by Yogesh Khedkar

Clive Two.Zero 

barkin.tyler.001

 

Hi Clive , 

I'm using the STM32F072 discovery board. In that i'm using the CAN peripherals CAN_Tx and CAN_Rx .

Below is the circuit diagram of my connection.

 

 

 I'm using MCP2551 trans-receiver. when i'm trying to send the CAN frame i'm getting the "bit dominant error".   

I have monitored the CAN_ESR (CAN error status register) in that Last error code (LEC) i got the count 101=> which indicates the "Bit dominant error". I'm not understanding the what goes wrong , i have shared the code also please help me if any body is having the solution for this.

 

CODE

---------------------------------------------------------------

 

 

/* Includes ------------------------------------------------------------------*/
#include "stm32f0xx.h"

/** @addtogroup STM32F0_Snippets
* @{
*/

/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
#define CMD_TOGGLE (0xDA)
#define CAN_ID_MASK (0xFF70U)
#define CAN_ID1 (0x651U)
#define CAN_ID2 (0x652U)
#define FILTER_LIST (1) /* 0: filter mode = identifier mask, 1: filter mode = identifier list */

/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/
/* Private function prototypes -----------------------------------------------*/
void Configure_GPIO_LED(void);
void Configure_GPIO_CAN(void);
void Configure_CAN(void);
void Configure_GPIO_Button(void);
void Configure_EXTI(void);

/* Private functions ---------------------------------------------------------*/

/**
* @brief Main program.
* @param None
* @retval None
*/
int main(void)
{

 

Configure_GPIO_LED();
Configure_GPIO_CAN();
Configure_CAN();
Configure_GPIO_Button();
Configure_EXTI();

/* Infinite loop */
while (1)
{
}
}


__INLINE void Configure_GPIO_LED(void)
{
/* Enable the peripheral clock of GPIOC */
RCC->AHBENR |= RCC_AHBENR_GPIOCEN;

/* Select output mode (01) on PC8 and PC9 */
GPIOC->MODER = (GPIOC->MODER & ~(GPIO_MODER_MODER8 | GPIO_MODER_MODER9)) \
| (GPIO_MODER_MODER8_0 | GPIO_MODER_MODER9_0);
}


__INLINE void Configure_GPIO_CAN(void)
{
/* Enable the peripheral clock of GPIOA */
RCC->AHBENR |= RCC_AHBENR_GPIOAEN;

/* GPIO configuration for CAN signals */
/* (1) Select AF mode (10) on PA11 and PA12 */
/* (2) AF4 for CAN signals */
GPIOA->MODER = (GPIOA->MODER & ~(GPIO_MODER_MODER11 | GPIO_MODER_MODER12))\
| (GPIO_MODER_MODER11_1 | GPIO_MODER_MODER12_1); /* (1) */
GPIOA->AFR[1] = (GPIOA->AFR[1] &~ (GPIO_AFRH_AFRH3 | GPIO_AFRH_AFRH4))\
| (4 << (3 * 4)) | (4 << (4 * 4)); /* (2) */
}

/**
* @brief This function configures CAN.
* @param None
* @retval None
*/
__INLINE void Configure_CAN(void)
{
/* Enable the peripheral clock CAN */
RCC->APB1ENR |= RCC_APB1ENR_CANEN;


CAN->MCR |= CAN_MCR_INRQ; /* (1) */
while((CAN->MSR & CAN_MSR_INAK)!=CAN_MSR_INAK) /* (2) */
{
/* add time out here for a robust application */
}
CAN->MCR &=~ CAN_MCR_SLEEP; /* (3) */
// CAN->BTR |= CAN_BTR_LBKM | 2 << 20 | 3 << 16 | 5 << 0; /* (4) */

CAN->BTR |= 2 << 20 | 3 << 16 | 5 << 0; /* (4) */
CAN->MCR &=~ CAN_MCR_INRQ; /* (5) */
while((CAN->MSR & CAN_MSR_INAK)==CAN_MSR_INAK) /* (6) */
{
/* add time out here for a robust application */
}
CAN->FMR = CAN_FMR_FINIT; /* (7) */
CAN->FA1R = CAN_FA1R_FACT0; /* (8) */
#if (FILTER_LIST)
CAN->FM1R = CAN_FM1R_FBM0; /* (9) */
CAN->sFilterRegister[0].FR1 = CAN_ID2 << 5 | CAN_ID1 << (16+5); /* (10) */
#else
CAN->sFilterRegister[0].FR1 = CAN_ID1 << 5 | CAN_ID_MASK << 16; /* (11) */
#endif /* FILTER_LIST */

CAN->FMR &=~ CAN_FMR_FINIT; /* (12) */
CAN->IER |= CAN_IER_FMPIE0; /* (13) */

/* Configure IT */
/* (14) Set priority for CAN_IRQn */
/* (15) Enable CAN_IRQn */
NVIC_SetPriority(CEC_CAN_IRQn, 0); /* (16) */
NVIC_EnableIRQ(CEC_CAN_IRQn); /* (17) */
}


__INLINE void Configure_GPIO_Button(void)
{
/* Enable the peripheral clock of GPIOA */
RCC->AHBENR |= RCC_AHBENR_GPIOAEN;

/* Select mode */
/* Select input mode (00) on PA0 */
GPIOA->MODER = (GPIOA->MODER & ~(GPIO_MODER_MODER0));
}

/**
* @brief This function configures EXTI.
* @param None
* @retval None
*/
__INLINE void Configure_EXTI(void)
{

SYSCFG->EXTICR[0] = (SYSCFG->EXTICR[0] & ~SYSCFG_EXTICR1_EXTI0) | SYSCFG_EXTICR1_EXTI0_PA; /* (1) */
EXTI->IMR |= EXTI_IMR_MR0; /* (2) */
EXTI->RTSR |= EXTI_RTSR_TR0; /* (3) */
NVIC_SetPriority(EXTI0_1_IRQn, 0); /* (4) */
NVIC_EnableIRQ(EXTI0_1_IRQn); /* (5) */
}

/******************************************************************************/
/* Cortex-M0 Processor Exceptions Handlers */
/******************************************************************************/

/**
* @brief This function handles NMI exception.
* @param None
* @retval None
*/
void NMI_Handler(void)
{
}

/**
* @brief This function handles Hard Fault exception.
* @param None
* @retval None
*/
void HardFault_Handler(void)
{
/* Go to infinite loop when Hard Fault exception occurs */
while (1)
{
}
}

/**
* @brief This function handles SVCall exception.
* @param None
* @retval None
*/
void SVC_Handler(void)
{
}

/**
* @brief This function handles PendSVC exception.
* @param None
* @retval None
*/
void PendSV_Handler(void)
{
}

/**
* @brief This function handles SysTick Handler.
* @param None
* @retval None
*/
void SysTick_Handler(void)
{
}


/**
* @brief This function handles EXTI 0 1 interrupt request.
* @param None
* @retval None
*/
void EXTI0_1_IRQHandler(void)
{
EXTI->PR |= 1;

if((CAN->TSR & CAN_TSR_TME0) == CAN_TSR_TME0)/* check mailbox 0 is empty */
{
CAN->sTxMailBox[0].TDTR = 1; /* fill data length = 1 */
CAN->sTxMailBox[0].TDLR = CMD_TOGGLE; /* fill 8-bit data */
CAN->sTxMailBox[0].TIR = (uint32_t)(CAN_ID1 << 21 | CAN_TI0R_TXRQ); /* fill Id field and request a transmission */
}
else
{
CAN->TSR |= CAN_TSR_ABRQ0; /* abort transmission if not empty */
}
}

/**
* @brief This function handles CAN interrupt request.
* @param None
* @retval None
*/
void CEC_CAN_IRQHandler(void)
{
uint32_t CAN_ReceiveMessage = 0;

if((CAN->RF0R & CAN_RF0R_FMP0)!=0)/* check if a message is filtered and received by FIFO 0 */
{
CAN_ReceiveMessage = CAN->sFIFOMailBox[0].RDLR; /* read data */
CAN->RF0R |= CAN_RF0R_RFOM0; /* release FIFO */
if((CAN_ReceiveMessage & 0xFF) == CMD_TOGGLE)
{
GPIOC->ODR ^= GPIO_ODR_8; /* Toggle orange LED */
}
}
}


/**
* @}
*/@@@@@@@@@@

Outcomes