AnsweredAssumed Answered

Simple remote control using STM8L001J3

Question asked by Sisto Zànier on May 18, 2018
Latest reply on May 19, 2018 by Sisto Zànier

Hi, I would like to use the SWIM port of STM8L001J3 to control an LED.
Obviously the same port will also need to be used for debugging and programming.
I ask if it is possible to connect the LED directly to the port or if is it better to use a MOS-N (2N7002) to avoid impedance problems?
I attach the schematic of the solution with MOS-N.

 

Thank you for your valuable feedback and suggestions

Sisto

Attachments

Outcomes