AnsweredAssumed Answered

MC SDK4.3 PWM frequency >65kHz

Question asked by thomas.greg.002 on May 18, 2018

I would like to run the Sensorless FOC firmware with a PWM frequency greater than 65kHz.

My hardware configuration:

Nucleo-F446RE -> X-Nucleo-IHM09M1 -> Custom power-stage with ICS current sensors and bus voltage measurement.

 

My software configuration:

ST MC SDK4.3 -> STM32F4xx_MC Library -> STM32F4xx_UserProject - SM32446E-EVAL

IAR Embedded Workbench IDE

 

I have successfully configured, compiled, uploaded and tested the sensorless FOC firmware with a PWM frequency of 30kHz. However, once the PWM frequency is increased above 65kHz, the compiler produces a number of warnings, and the controller is not able to drive the test motor.

 

I have inspected the source code for the firmware. The PWM_FREQUENCY is declared in Drive_parameters.h, with no type. All subsequent calls cast the value to uint16_t, which explains the 65kHz limit.

I have attempted to change the declaration of variables that will take the PWM_FREQUENCY and TF_REGULATION_RATE to uint32_t. I have worked through the variables one-by-one to check that everything still works with a PWM frequency of 30kHz. I can change all calls apart from one:

Once I change the 'hMeasurementFrequency' member of the SpeednPosFdhkParams_t structure in SpeedNPosFdbkClass.h from uint16_t to uint32_t, the code will compile but the motor will not run. I have unsuccessfully tried to identify operations that use .hMeasurementFrequency and determine why they won't work with a uint32_t value.

 

I would be incredibly grateful if someone with a more in-depth understanding of the SDK (and software debugging in general) would be able to assist me with figuring out how to modify the code.

 

Thank you in advance!

Greg

Outcomes