AnsweredAssumed Answered

CPAL I2C Issue

Question asked by hudgell.michael on Apr 12, 2012
Latest reply on Feb 14, 2015 by dmitriy.ivanov
One of my colleague has an issue with CPAL that ppl might have seen before (when being used for I2C communication on the SMT32L15R6...

It appears to do start communicating, sends the start, sends the address and then gets an ack back. the SCLK line is then help low for a significant amount of time (~25ms) and then the communications carries on without any issue.

The communication appears to happen OK, but obviously this delay is unfortunate...

Outcomes