AnsweredAssumed Answered

LIS3DH ADC Interrupt

Question asked by pj chow on May 17, 2018
Latest reply on May 22, 2018 by Miroslav B

Hello,

     checked the lis3dh manual, there is such a sentence “ The status of the 321DA bit can be driven to the INT1 pad by setting the I1_DRY2 bit of CTRL_REG3 to 1.” ,I have do it(ADC_PD bit of TEMP_CFG_REG (1Fh) to 1, ODR bit of CTRL_REG1(20h)  to 1HZ ), but can’t get interruptes signals.INT1 pin is always high. other work well.

 

 

Thanks for your help.

Outcomes