AnsweredAssumed Answered

Doubts about <feature> TAG within a new BSP PDSC file

Question asked by fernando maldonado on May 15, 2018

Hi Everyone!

 

   I'm developing a BSP file -board support package,  for a personal purpose card ' ad hoc ', using the STM32H753XI.

   While creating the PDSC file -pack description software component, I needed to include some TAGS <features> within TAG <board> threat.

   To take a secure reference, I used as a template the PDSC of the STM32H743I-EVAL, in its recent new version 2.1.0.

   There I found some <feature>, that perhaps I don't understand as correctly are like as how important are, after checking them all -in the reference file mentioned before STM32H743I-EVAL Datasheet.

   Then, through this post I'm sharing my doubts with st dot com Community, to know if some <feature> TAGS  within the reference PDSC file... are they really correct or needed.

 

      ... 

      ...

      <mountedDevice deviceIndex="0" Dvendor="STMicroelectronics:13" Dname="STM32H743XI"/>
      <compatibleDevice deviceIndex="0" Dvendor="STMicroelectronics:13" DsubFamily="STM32H743"/>
      <feature type="ODbg" n="1"     name="On-board ST-LINK/V2"/>
      <feature type="RAM" n="1"       name="8M x 32-bit SDRAM"/>
      <feature type="RAM" n="1"       name="1M x 16-bit SRAM"/>
      <feature type="ROM" n="1"      name="8M x 16-bit Nor Flash"/>
      <feature type="ROM" n="1"      name="512-Mbit Quad-SPI NOR Flash"/>

      Is it right? I think isn't complatible with the STM32H743I-EVAL Datasheet

 

      <feature type="USB" n="1"       name="High-Speed USB with micro-AB Connector"/>
      <feature type="USB" n="2"       name="Full-Speed USB with micro-AB Connector"/>
      <feature type="Joystick" n="1" name="5-position Joystick"/>
      <feature type="Camera" n="1"/>
      <feature type="Button" n="2"    name="Push-Buttons for Reset, Wakeup/Tamper or Key"/>
      <feature type="LED"                  n="4" name="4 color user LEDs"/>

 

      <feature type="GLCD" n="1" m="800.480" name="4-inch 800x480 TFT color LCD with capacitive touch panel"/>

      Is it right? I think isn't complatible with the STM32H743I-EVAL Datasheet for the 5.7 inch TFT 640x480

 

      <feature type="Poti" n="1"         name="Analog Voltage Control for ADC Input (potentiometer)"/>
      <feature type="LineIn" n="1"     name="Audio CODEC with Stereo Line-In/Out and Speaker/Microphone"/>
      <feature type="LineOut" n="1"  name="Audio CODEC with Stereo Line-In/Out and Speaker/Microphone"/>
      <feature type="MIC"                  n="2" name="ST MEMS microphones"/>
      <feature type="Speaker"           n="2"/>
      <feature type="Other"               n="1" name="Digital Stereo Microphone"/>
      <feature type="CAN"                 n="1"/>
      <feature type="RS232"             n="1"/>
      <feature type="I2C" n="4"/>
      <feature type="ETH"                 n="1" name="10/100 Ethernet Port"/>
      <feature type="XTAL"               n="25000000"/>
      <feature type="PWR"               n="5" name="USB Powered"/>
      <feature type="PWR"               n="3" m="5" name="External Supply"/>
      <feature type="MemCard"        n="1" name="SDIO interface microSD card"/>

 

      <feature type="DIO" n="34" name="Motor Control Connector"/>

      Is it right? I think isn't complatible with the STM32H743I-EVAL Datasheet

 

      <feature type="DIO" n="60" name="Daughterboard Extension header 1"/>
      <feature type="DIO" n="60" name="Daughterboard Extension header 2"/>

 

      <feature type="ConnOther" n="1" name="Motor control connector"/>

      Is it right? I think isn't complatible with the STM32H743I-EVAL Datasheet

 

      <debugInterface adapter="ST-Link" connector="Mini-USB"/>
      <debugInterface adapter="JTAG/SW" connector="20 pin JTAG (0.1 inch connector)"/>
      <debugInterface adapter="JTAG/SW" connector="20-pin Cortex debug + ETM Trace (0.05 inch connector)"/>
</board>

 

   Community of st dot com, please, Can you help me with my doubts? Every kind of post will be welcome!

 

   fernando maldonado

   Argentina

Outcomes