AnsweredAssumed Answered

FREERTO

Question asked by ABDELAOUI samira on May 14, 2018
Latest reply on May 24, 2018 by Clive Two.Zero
Branched from an earlier discussion

Hello Imen,

 

Can you help me in the interruption configuration of stm32479I eval board

how to configure the freertos interruption please ??

When I debug it blocks in the hal_delay function exactly in the while loop

__weak void HAL_Delay(uint32_t Delay)

{

uint32_t tickstart = HAL_GetTick();

uint32_t wait = Delay;

 

/* Add a freq to guarantee minimum wait */

if (wait < HAL_MAX_DELAY)

{

wait += (uint32_t)(uwTickFreq);

}

 

while((HAL_GetTick() - tickstart) < wait)

{

}

}

 

 

2018-05-14 18:02 GMT+02:00 Imen D <st-microelectronics@jiveon.com>:

 

STMicroelectronics Community

<https://community.st.com/?et=watches.email.thread>

Re: SDMMC trace length mismatch

 

reply from Imen D

<https://community.st.com/people/DAHMEN.IMEN?et=watches.email.thread> in *STM32

MCUs Forum* - View the full discussion

<https://community.st.com/message/197360-re-sdmmc-trace-length-mismatch?commentID=197360&et=watches.email.thread#comment-197360>

Outcomes