AnsweredAssumed Answered

End of program...

Question asked by M G on May 12, 2018
Latest reply on May 17, 2018 by Clive One

Dear Community,

 

If I compile a project for e.g. STM32F051 which contains following line

int END_ofProg              __attribute__((at(0x08007C00)))     = 1; supposed to show up at the end of program, then I notice that Keils’ compiler adds some additional stuff on top of the hex dump:

 

:107C00000100000000000000000000000000000073

:107C10000000000000000000000000000000000064

:107C20000000000000000000000000000000000054

:107C30000000000000000000000000000000000044

:107C40000000000000000000000000000000000034

:107C50000000000000000000000000000000000024

:107C60000000000000000000000000000000000014

:107C70000000000000000000000000000000000004

:107C800000000000000000000000000000000000F4

:107C900000000000000000000000000000000000E4

:107CA00000000000A92E0008B92D00081D2E0008B4

:107CB000F12E000800000000011200084D1200081B

:107CC000F91B000800000000010203040102030484

 

If I remove this additional code later on e.g. by deleting the associated flash page the code stops to work after reset. If I look for the map file the code inside the hex dump should not to be there.

 

    0x08006868   0x00000008   Data   RW           61    .ARM.__AT_0x08006868  main.o

    0x08006870   0x00001390   PAD

    0x08007c00   0x00000004   Data   RW           62    .ARM.__AT_0x08007C00  main.o **

** this is the last line.

 

After searching the ST Forum regarding this this issue Ive found this Thread: https://community.st.com/message/3170

However I not really understand what the mentioned change of the scatter file really does and if a changed scatter file will cause that the additional code vanishes.  I would be glad if someone would post a more descriptive explanation of what is going on.

 

 

 

Outcomes