AnsweredAssumed Answered

STM32F412G-DISCO arduino pin assignment error

Question asked by Adam Hamilton on May 9, 2018
Latest reply on May 16, 2018 by houda ghabri

When I create a project in CubeMX 4.25.0 with the STM32F412G-DISCO board, the arduino pin assignments are all wrong.

I have attached a partial screenshot of the CubeMX project showing the incorrect assignment and a screenshot of the user manual's pin assignment.

CubeMX Pin Assignment

 

Datasheet Pin Assignment

 

Is this likely to be corrected in a future update?

 

I don't think this is likely to cause problems as enabling the USART6 peripheral, for example, can't be set to D0 and D1 (PD14 & PD15) in CubeMX but it does cause a bit of confusion when trying to assign peripherals.

 

Kind regards

Adam Hamilton

Outcomes