AnsweredAssumed Answered

SPC560B Discovery board , Issue with stop mode .

Question asked by Alok Nigam on May 10, 2018
Latest reply on May 15, 2018 by Erwan Y

I am using spc560b discovery board , i want to implement low power modes like halt , stop and standby ,

i am able to implement standby mode and waking up with CAN Rx at PB1 , however when i try with stop mode

i think it got hang and current consumption not get reduced and it didn't wakeup like in standby mode .

 

For sleep i am using PA3 pin interrupt , most of the code i have took from the example project , SPC560Bxx_OS-Less_STANDBY_Test_Application_for_Discovery that i got in different thread .

 

I am sharing code as attachment any help will be appreciated .

Attachments

Outcomes