AnsweredAssumed Answered

HAL_CAN_Init() is failing

Question asked by n.serina on May 8, 2018
Latest reply on May 9, 2018 by T J

Hi, 

I was just started with CAN peripheral on my stm32f446re nucleo board. 

The problem i am facing is HAL_CAN_Init()  added by cubeMx code generation software is failing at the below line of code 

it is returning HAL_ERROR in CAN1 LOOP BACK MODE

That means the controller has not set SLAK to zero even if we clear the SLEEP bit 

 

i believe that CAN TX is internally connected to can rx and can rx is not sampled . 

on the board i have made no connection to the can tx and can rx. its just a single board. 

Please let me know what i am doing wrong . 

 

 

/* Exit from sleep mode */
CLEAR_BIT(hcan->Instance->MCR, CAN_MCR_SLEEP);

/* Get tick */
tickstart = HAL_GetTick();

/* Check Sleep mode leave acknowledge */
while ((hcan->Instance->MSR & CAN_MSR_SLAK) != RESET)
{
if ((HAL_GetTick() - tickstart) > CAN_TIMEOUT_VALUE)
{
/* Update error code */
hcan->ErrorCode |= HAL_CAN_ERROR_TIMEOUT;

/* Change CAN state */
hcan->State = HAL_CAN_STATE_ERROR;

return HAL_ERROR;
}

 

here is picture of all reg contents 

Outcomes