AnsweredAssumed Answered

How to divide RAM into 2 sections in stm32f4

Question asked by bhargavi ale on May 7, 2018
Latest reply on May 11, 2018 by Clive Two.Zero

Hi All,

Am trying to fix the RAM addresses for new global variables in .data segment. For this, I have divided RAM into sections and by using attribute Am fixing address for newly created global variable. It was looks fine, but newly added global variables are not initializing with default value i.e., 0 and it is persistent variables also getting affect i.e., after reset, persistent variables are initializing with zero instead of retaining the value.

 

I have created RAM sections like below,

In linker script:

RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 120K
RAM2 (xrw) : ORIGIN = 0x20000000 + 120K, LENGTH = 8K

 

.data :
{
. = ALIGN(4);
_sdata = .; /* create a global symbol at data start */
*(.data) /* .data sections */
*(.data*) /* .data* sections */

. = ALIGN(4);
_edata = .; /* define a global symbol at data end */
} >RAM AT> FLASH

.data_user :
{
. = ALIGN(4);
_sdata_user = .; /* create a global symbol at data start */
*(.data_user) /* .data sections */
*(.data_user*) /* .data* sections */

. = ALIGN(4);
_edata_user = .; /* define a global symbol at data end */
} >RAM2 AT> FLASH

 

In startup code, I have added few instructions to initialize new global variables to 0.

movs r1, #0
b LoopCopyDataInit
b LoopCopyUserDataInit

CopyDataInit:
ldr r3, =_sidata
ldr r3, [r3, r1]
str r3, [r0, r1]
adds r1, r1, #4

LoopCopyDataInit:
ldr r0, =_sdata
ldr r3, =_edata
adds r2, r0, r1
cmp r2, r3
bcc CopyDataInit
ldr r2, =_sbss
b LoopFillZerobss
/* Zero fill the bss segment. */
FillZerobss:
movs r3, #0
str r3, [r2], #4

LoopFillZerobss:
ldr r3, = _ebss
cmp r2, r3
bcc FillZerobss

CopyUserDataInit:
ldr r7, =_sdata_user
ldr r7, [r7, r5]
str r7, [r4, r5]
adds r5, r5, #4

LoopCopyUserDataInit:
ldr r4, =_sdata_user
ldr r7, =_edata_user
adds r6, r4, r5
cmp r6, r7
bcc CopyUserDataInit
ldr r6, =_sdata_user
bcc LoopFillZeroUserData

FillZeroUserbss:
movs r7, #0
str r7, [r6], #4

LoopFillZeroUserData:
ldr r7, = _edata_user
cmp r6, r7
bcc FillZeroUserbss

 

In .c file:

__attribute__((section(".user_data"))) int DebugEx1 = 0; // new global variable.

RAM address for DebugEx1 is came inside .user_data section but, facing above bugs.

Please, Help me out from this problem

 

regards,

Bhargavi Ale.

Outcomes