AnsweredAssumed Answered

STM32F417IG board not enumerating as com port

Question asked by de.sa on Oct 28, 2014
Latest reply on Oct 29, 2014 by Clive One
Hi,

I built a .bin file configured to make the chip run as VCP. I flashed the .bin using busblaster successfully.

I get the following message after flashing via openocd
wrote 26284 bytes from file STM32DiscoveryVCP-master/STM32_Build/Debug/bin/build.bin to flash bank 0 at offset 0x00000000 in 0.537990s (47.711 KiB/s)
 

But, when I connect the board to USB and check for devices in Device Manager. It does not show up as com port. It is enumerating as STMicroelectronics STM32 BOOTLOADER [2200].

Even though I toggle the switch between bootloader and flash. It is only recognizing bootloader. I tried setting BOOT 0 to high but still no difference.

Please suggest any solution.


Thanks

Outcomes