AnsweredAssumed Answered

L6227Q using Enable as PWM signal

Question asked by Peter Fournier on May 4, 2018
Latest reply on May 21, 2018 by Enrico Poli

The L6227Q looks like just the part I want to control a small motor that will run at about 5V and no more than 300mA.  I was looking at Table 7 in the data sheet.  I think what I want is to set IN1 and IN2 to the polarity I need  and then use the ENABLE line as the PWM signal to adjust the speed.  Does this sound reasonable?

 

Thanks,

-Pete 

Outcomes