AnsweredAssumed Answered

flashing stm32F303 based custom board

Question asked by Channamallesh Hiremath on May 3, 2018

Hello,

 

I am making a custom board based on STM32F3 discovery board. My custom board is an exact copy of the discovery board with additional sensor components. 

 

I can easily program STM32F3 board as st-link is already built on to the board. 

How do I do the same thing when I get my boards done?

 

I do have both  STM32F103C8T6  processor and  STM32F303VCT6 on the system.

 

Is there a code for STM32F103C8T6 which I can use to flash the board? 

 

Can you please help me with this?

 

Best Regards,

 

Mallesh 

Outcomes