AnsweredAssumed Answered

LMX358IQ2T Output Current Capability

Question asked by Dave Kearney on May 3, 2018
Latest reply on Jun 28, 2018 by AUPETIT nicolas

Hi, I'm looking for an op-amp to buffer a signal and provide an output of 2 -> 5V to a load of 100 - 200R. This would require driving the load with 50 - 100 mA. The LMX358IQ2T has a specified output source current of 60-70 mA, but I'm not sure if this just means an absolute max or a max where the output voltage signal will be maintained? Will the voltage output have degraded substantially at roughly this current? If so, what are my options for op-amps capable of driving 50-100mA over 2-5V without significant degradation?

Many Thanks,

Dave

Outcomes