AnsweredAssumed Answered

STM32CubeMX generated code doesn't run on STM32l496 Nucleo-144 board

Question asked by Dick Lin on May 3, 2018
Latest reply on May 17, 2018 by Clive One

Hi,

I am using STM32CubeMX generated code run on Nucleo-144 board for STM32L496ZGT MCU. When I just have 3 UART enabled in cube, the code seems work fine. After I have added more components to the cube, the code go to an startup_stm32l4a6xx.s code. Seems a exception.

 

Here is the init code. The issue starting MX_LPUART1_UART_Init(). If I comment this out, will exception other init code too.

 

Any thoughts on this failure?

 

Thanks,

****

 

/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ADC1_Init();
MX_ADC3_Init();
MX_AES_Init();
MX_CRC_Init();
MX_HASH_Init();
MX_I2C1_Init();
MX_I2C2_Init();
MX_IWDG_Init();
MX_LPUART1_UART_Init();
MX_UART4_Init();
MX_UART5_Init();
MX_USART1_UART_Init();
MX_USART2_UART_Init();
MX_USART3_UART_Init();
MX_QUADSPI_Init();
MX_RNG_Init();
MX_RTC_Init();
MX_SPI1_Init();
MX_SPI2_Init();
MX_WWDG_Init();

 

 

 

 

/* Zero fill the bss segment. */
FillZerobss:
movs r3, #0
str r3, [r2], #4

LoopFillZerobss:
ldr r3, = _ebss
cmp r2, r3
bcc FillZerobss

Outcomes