AnsweredAssumed Answered

How to change the Display Language of an LCD from Korean to English

Question asked by Jawad Waheed on May 2, 2018
Latest reply on May 3, 2018 by Dan Mackie

I have a machine with an LCD display that is in Korean, I want to change that to English. Following are the details. 

 

There is this LCD Module with Toshiba T6963C Controller, which is bus connected to a PCB that has a ST PSD913F2-90J and a DS80C320 Microcontroller embedded on it, and only a JTAG connector IEEE1149.1 ( enabling only 4 pins : TDO, TDI, TCK, TMS) ... as the display is in Korean, the LCD controller T6963C is using a custom External Memory to read characters, most probably ST PSD913F2-90J, so my question was how to access this PSD913F2 and change where ever that Korean Display data is stored into English. Assistance would be highly appreciated. 

Outcomes