AnsweredAssumed Answered

LIS3DH temperature sensor when supply voltage is 1.8V

Question asked by L CO on May 2, 2018
Latest reply on May 4, 2018 by L CO

Hello,

 

I have a question regarding a note in the datasheet of the LIS3DH accelerometer:

 

I want to use the accelerometer LIS3DH for one of my application with the following specifications:

- The accelerometer is supplied at 1.8V (in compliance with datasheet).

- The functions to be achieved are: orientation detection and  provide temperature.

 

I saw the following note in the datasheet:

"The product is factory calibrated at 2.5 V. Temperature sensor operation is guaranteed in the range 2 V - 3.6 V."

 

What those that means? The temperature sensor is not working when the accelerometer is supplied at 1.8V ?

 

Thanks for your help.

Outcomes