AnsweredAssumed Answered

Can't Detect Execution of Query Command ST25RU3993

Question asked by Tiago Santos on May 2, 2018

Hi,

 

I am developing a product based on the AS3993, AKA ST25RU3993. I have been using the FEMTO module (by AMS) to test my application code.

So far I was able to verify the initialization, SPI, interrupt line, cristall stabilization and PLL lock. Everything seems to be OK.

I am now trying to read a TAG.

Using the defautl configurations of the FEMTO, as follow:

 

Gen 2 Related Register ST25RU3993

 

In order to start reading a tag. I first write the values above in the registers, then I enable the bit RF_ON on register 0x00.

After send the Query command 0x98 and write the following bytes to the FIFO:

 

//0b00
//dr = 0b01
//m = 0b10
//Trext = 0b00

0x18

 

//sel = 0b00
//session = 0b00
//target = 0b00
//q = 0b00

0x00

 

After that I start to wait for the end of tx interrupt, but I detect a irq_noresp instead.

Any insights?

Outcomes