AnsweredAssumed Answered

Use stm32f3discovery.cfg, Connection Failed, STM32F302 Nucleo with openOCD ?

Question asked by Tension on Oct 28, 2014
Latest reply on Oct 30, 2014 by nouha
Terminal says:

Open On-Chip Debugger 0.8.0 (2014-04-28-08:42)
Licensed under GNU GPL v2
For bug reports, read
        http://openocd.sourceforge.net/doc/doxygen/bugs.html
Info : This adapter doesn't support configurable speed
Info : STLINK v2 JTAG v21 API v2 SWIM v5 VID 0x0483 PID 0x374B
Info : using stlink api v2
Info : Target voltage: 3.250693
Info : stm32f3x.cpu: hardware has 6 breakpoints, 4 watchpoints
Info : accepting 'gdb' connection from 3333
Info : device id = 0x10016439
Warn : Cannot identify target as a STM32 family.
Error: auto_probe failed
Error: Connect failed. Consider setting up a gdb-attach event for the target to prepare target for GDB connect, or use 'gdb_memory_map disable'.
Error: attempted 'gdb' connection rejected


Outcomes