AnsweredAssumed Answered

i need to connect two stm32 udp with a switch to pc

Question asked by TARHAN SAMAH on Apr 26, 2018
Latest reply on May 2, 2018 by Clive One

hello when i connect two stm32 one ip 10.1.1.88 port 88 the other one is 10.1.1.70  port 70  to a with switch device using udp to a remote pc ethernet   ip  10.1.1.89   , if one send data the other stm cannot send ???? separatly they can work very good 

 

on the same time they cannot work ?? 

 

 do i need a special switch for that ??? which one 

 

thanks 

Outcomes