AnsweredAssumed Answered

XNUCLEO-IDW04A1 WIFI with SPI

Question asked by plante.raphael on Apr 25, 2018

Hi,

I want to connect to the wifi board XNUCLEO-IDW04A1 with my nucleo stm32l476RG developpment board. However I am getting a strange behaviour similar to what is posted on Yet another SPI SPWF04S problem  except that I get the problem at the beginning of the example Client_Socket in the x-cube-wifi1_firmware.V3.1.1. I used the latest firmware SPWF04S-171117-0328fe3-Full.hex for the wifi board. The program get stucked at line 433 of wifi_interface.c

 while(IO_status_flag.WiFi_WIND_State!= WiFiPowerDown);//Till +WIND:38:WiFi Powered Down arrives

Thank you

 

 

/********************************************************
 *                                                      *
 * X-CUBE-WIFI1 Expansion Software v3.1.1               *
 * X-NUCLEO-IDW0xx1 Wi-Fi Configuration.                *
 * Client-Socket Example                                *
 *                                                      *
 *******************************************************/

 

Do you want to setup SSID?(y/n):n

 

 

 

 Module will connect with default settings.

 

/**************************************************************
 * Configuration Complete                                     *
 * Port Number:32000, Protocol: TCP/IP                        *
 * Please make sure a server is listening at given hostname   *
 *************************************************************/

 


Initializing the wifi module...

 

Build Configuration:
Nucleo: NUCLEO-L476RG
X-Nucleo: X-NUCLEO-IDW04A1
Interface: SPI

 

>> Configuration Failure no 2
<<WIND 7, status 0

 

<<WIND 1, status 0

 

<<WIND 13, status 0

 

<<WIND 3, status 0

 

<<WIND 0, status 0

 

<<WIND 32, status 3

 

>>AT+S.SCFG

 

<<OK

 

>>AT+S.FCFG

 

<<OK

 

>>AT+S.WCFG

 

<<OK

 

>> Configuration Failure no 2
<<WIND 7, status 0

 

<<WIND 1, status 0

 

<<WIND 13, status 0

 

<<WIND 3, status 0

 

<<WIND 0, status 0

 

<<WIND 32, status 3

 

WiFi Initialised and Ready..

 

>>AT+S.WIFI

 

<<OK

Outcomes