AnsweredAssumed Answered

Delta to WYE three phase voltages conversion

Question asked by hexfet13 on Apr 24, 2018
Latest reply on Apr 25, 2018 by AvaTar

Hello to all,

 

I'm here to ask a question about the energy meter I've developed.

 

The problem concerns the 3P3W system (neutral line not available).

 

In this case i can measure two line to line voltages and the phase between them to reconstruct the ideal 3 vectors system(with a ideal phase of 120° between phases).

 

The main problem is that the alghorithm i developed is too slow on an stm32 M4 @80Mz: in a worst case it takes about 60ms to find the 3 vectors who generate the aquired two line to line voltage measurements and their phase displacement (with an acceptable error).

 

I searched a lot without founding a method to reconstruct  3P4W from a 3P3W system(unbalanced); the uniqe useful documents i've found is this one: Calculating Line-to-Line Voltages from Line-to-Neutral Measurements with the NI 9225 - National Instruments
and is the same method i developed to construct my slow algorithm(it does a convergence to find the solution to the problem)

 


The question is: there's somewhere a relation or a library already developed than convert a DELTA three phase system to WYE ones just passing 2 vectors and the phase displacement?
Thanks!

Outcomes