AnsweredAssumed Answered

Export Example Includes Linked Files

Question asked by Jules A on Apr 24, 2018
Latest reply on Apr 25, 2018 by Jules A

Hello,

 

I'm trying to export an example project for the STM32F429I-EVAL1 (to work on it).

 

The example works fine but when I export it :

- Either I get all the directories and the .c files BUT no includes at all

or 

- I get all the directories but no files at all.

I know that it's using links from the .cproject (& .project) but I just want to dissociate the project from the rest of the examples so that I can work on it separately. (and not have all those directories at the root of my working folder like it's the case in the cubemxf4 folder).

 

Edit : I'm using Atollic TrueStudio to work (and do the exports)

 

Thanks for your help

 

Jules

Outcomes