AnsweredAssumed Answered

The mc workbench 'MCSDK 5.0.3(2)' doesn't see STM32CUBEMX (the latest version) !!

Question asked by gokay aygok on Apr 20, 2018
Latest reply on May 3, 2018 by PALANO Carmelo Marcello

Hello dear ST community members, 
I am so sorry to ask this question for a couple of times. But, I don't have any other choice.

 

I have installed the motor control workbench and STM32CUBEMX. However, I can not generate the code for motor control. The error is, NO STM32CUBEMX version above 4.25.0 has been found. Is there any version of cubemx which is newer than 4.25.0 ?

 

When I remove the STM32CUBEMX, I am getting the same error, too. Therefore, I came to the point that the motor control workbench MCSDK 5.0.3 and 5.0.2 do not see the latest version of cube mx, which is 4.25.0.

 

The screenshot of the error can be found in attached file.

 

Any help, idea, suggestion and advise would be appreciated.

 

Thanks a lot dear ST community members....

 

***I have gone through the installing steps for my all computer with windows 7 and 10 (32 and 64 bits). All results are the same.***

Attachments

Outcomes