AnsweredAssumed Answered

I got "Target power failure" error when I built a project

Question asked by Zhentao Lu on Apr 12, 2018
Latest reply on Apr 17, 2018 by Zhentao Lu

I bought a development board - STM3210C-SK/RAIS [Development Boards & Kits - ARM Raisonance]. I intalled the Ride 7 from the CD in the package, set up and confirmed all jumpers then opened an example - QuickStart_STM32F107. After I clicked the Project -> Build Project command, there is an error saying that "Target power failure: Measured 0.000000V.

 

There is a quick start manual.

 

The error:

 

In Debug options window, if I clicked “Connect to Debugger”, then:

 

I assume that the board has already connected with my computer.

 

This is my board:

 

I searched in google and found two websites talking about such error but their boards are not exactly same as my board.

 

Target power failure: Measured 0.100000V - problem on Windows XP
http://www.stm32circle.com/forum/viewtopic.php?id=86

 

Topic : I got "Target power failure" error when I built a project
http://support.raisonance.com/node/897559

 

It seems something goes wrong on my board. Does anyone have the same problem? Thank you very much.

 

Zhentao Lu

Outcomes