AnsweredAssumed Answered

How can i load .dfu file form the flas drive to my  STM3241G-EVAL Evaluation board

Question asked by Diwakar Ragupathy Raj on Apr 11, 2018
Latest reply on Apr 11, 2018 by Clive One

Hello,

 

The demonstration application for the  STM3241G-EVAL Evaluation board was erased and I am trying to reprogram it back using USB flash drive. I followed the steps and still was not able to see progress in the LCD.

1). Jumper configuration was checked as per the datasheet. But for the boot mode the BOOT0 and BOOT1 should be 1<->2 but I see on the board there is either 0 or 1. what should I do now? and please help me what should be the BOOT0 and BOOT1 be set to ?

2). I copied the dfu file to the flash drive and then connected it to the board using the Micro-AB to standard receptacle A connector to the USB OTG HS pin. Is it correct ?

Outcomes