AnsweredAssumed Answered

ST-Link CLI erase

Question asked by Jacek Stanaszek on Apr 11, 2018

ST-Link CLI rease another sector. 

STM32F767ZI, dual bank.

When using the commandline-switch -SE 15 st-link cli (v 3.2.0.0) reports:

ST-LINK Firmware version : V2J29S7
Connected via SWD.
SWD Frequency = 4000K.
Target voltage = 2.8 V.
Connection mode : Normal.
Device ID:0x451
Device flash Size : 2048 Kbytes
Device family :STM32F76x
Memory Sector @0x0810C000 erased

 

but erased sector 0x08108000.

 

Version 2.5.0 reports:

ST-LINK Firmware version : V2J29S7
Connected via SWD.
SWD Frequency = 4000K.
Target voltage = 2.8 V.
Connection mode : Normal.
Device ID:0x451
Device flash Size : 4095 Kbytes
Device family :STM32F76x
Memory Sector @0x0810C000 is not erased. Verify the memory protection.

 

Bank2 erase can resolve this problem.

Outcomes