AnsweredAssumed Answered

Missing SDRAM choice in STM32Cube for 100 pin package

Question asked by yaman.omer.002 on Apr 8, 2018
Latest reply on Apr 8, 2018 by yaman.omer.002

Hello everyone,

I want to use 100pin STM32F446 or STM32F722 microcontroller to drive an SDRAM. Bu in STM32Cube it doesn't have an SDRAM choice in FMC peripheral. When i select a 144pin version of these microcontrollers the SDRAM choice appears in STM32Cube.  So do i have to use a 144pin package to drive an SDRAM in FMC module instead of 100 pinned one

Outcomes